Now at Mouser: Fanstel's Compact BC15 Bluetooth 6.0 Modules for Wireless IoT, Smart Home, and VR/AR Applications

For Immediate Release

Connect With Us


Learn more about the BC15 Bluetooth 6.0 modules
Learn more about the BC15 Bluetooth 6.0 modules

March 19, 2026Mouser Electronics, Inc., the industry's leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components™, is now stocking the BC15 Bluetooth® 6.0 modules from Fanstel. The BC15, based on the Nordic nRF54L15 System-on-Chip (SoC), is a compact, Bluetooth Low Energy (LE) 6.0 module featuring an Arm® Cortex®-M33 microcontroller (MCU). The BC15 modules accelerate time-to-market for wireless Internet of Things (IoT) products, medical and smart home devices, remote and gaming controllers, and other applications.

The BC15 modules, now at Mouser, provide 1.524 MB of Flash, 256 KB of RAM, an embedded 2.4 GHz multiprotocol transceiver, and an integrated chip antenna or a u.FL for an external antenna. With Bluetooth 6.0, the BC15 modules support wireless connectivity while offering improvements in speed (up to 4 Mbps), latency (down to ~20ms), and range (up to 300m). The modules' stand-out features include channel sounding for high precision, UWB-like tracking, decision-based advertising for improved efficiency, and enriched LE Audio support.

The BC15 modules embed both 32 KHz crystals and DC-DC converter inductors. Requiring no external components, the BC15 modules enable faster time-to-market with lower development costs. The BC15 modules offer a range of platform security features, including secure/non-secure memory protection, a symmetric and asymmetric key crypto accelerator, tamper detection, and debug access port protection. The modules also feature an extensive range of peripherals, including two real-time counters (RTC), one global RTC (GRTC), seven 32-bit timers with counter mode, and near field communication (NFC), among others.

The BC15 Bluetooth 6.0 modules feature an operating temperature range of -40°C to +105°C. Development support for the BC15 modules is provided by the BC25 Bluetooth 6.0 EV-BC15x evaluation boards, also available from Mouser, with four variants available, tailored to each module version. The Nordic nRF54L15-DK development kit is required to program the boards.

To learn more, visit https://www.mouser.com/new/fanstel/fanstel-bc15-modules/.

For more Mouser news and our latest new product introductions, visit https://www.mouser.com/newsroom/.

 

As a global authorised distributor, Mouser offers the world's widest selection of the newest semiconductors and electronic components — in stock and ready to ship. Mouser's customers can expect 100% certified, genuine products that are fully traceable from each of its manufacturer partners. To help speed up the design process for customers, Mouser's website hosts an extensive library of technical resources, including a Technical Resource Centre, along with product data sheets, supplier-specific reference designs, application notes, technical design information, engineering tools and other helpful information.

About Mouser

2026 - Mouser Electronics is an authorized semiconductor and electronic component distributor focused on New Product Introductions from its leading manufacturer partners. Serving the global electronic design engineer and buyer community, the global distributor's website, mouser.com, is available in multiple languages and currencies and features more than 6.8 million products from over 1,200 manufacturer brands. Mouser offers 28 support locations worldwide to provide best-in-class customer service in local language, currency and time zone. The distributor ships to over 650,000 customers in 223 countries/territories from its 93,000m², state-of-the-art distribution facilities in the Dallas, Texas, metro area. For more information, visit https://www.mouser.com.

About Fanstel

2026 - Fanstel was established in 1990 as a caller ID products manufacturer, supplying major phone companies. Fanstel now uses its experience making high-quality telecom products to make hardware building blocks for transmitting sensor data and control signals between IoT devices and cloud services, smartphones, and computers. As a vertically integrated manufacturer, Fanstel offers certified open-source products in market-ready enclosures.

Trademarks

Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.

For further information, please contact:
Kevin Hess, Mouser
Senior Vice President of Marketing
+1 (817) 804-3833
For press enquiries, please contact:
Kelly DeGarmo, Mouser
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764