NXP Semiconductors' i.MX RT1180 Microcontrollers, Now at Mouser, Offer Advanced Security for Ethernet and Industry 4.0/5.0 Applications

New Product Announcement

Connect With Us


Learn more about the i.MX RT1180 Microcontrollers
Learn more about the i.MX RT1180 Microcontrollers

May 28, 2026Mouser Electronics, Inc., the industry's leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components™, is now stocking the i.MX RT1180 crossover microcontrollers (MCUs) from NXP® Semiconductors. The dual-core, real-time MCUs feature a high-performance Arm® Cortex®-M7 core operating at up to 800 MHz and a Cortex-M33 operating at up to 300 MHz. The NXP i.MX RT1180 MCUs are designed for a range of applications, including industrial and building automation, motion control and robotics, motor drives, programmable logic controllers and remote I/Os, and the Internet of Things (IoT).

The NXP i.MX RT1180 crossover MCUs, now available at Mouser, feature industrial gateway capabilities, supporting PROFINET®, EtherCAT®, EtherNet/IP™, and other industrial real-time protocols. The NXP i.MX RT1180 also offers professional networking stacks, following NXP's acquisition of port GmbH in 2025. The NXP i.MX RT1180 series also supports time-sensitive networking (TSN) protocols through a state-of-the-art Ethernet switch subsystem and 1.5 MB on-chip RAM protected by error-correcting code (ECC). The NXP i.MX RT1180 MCUs feature an integrated power management module with DC-DC and Low-Dropout (LDO) regulators, reducing the complexity of the external power supply and simplifying power sequencing. The MCUs offer advanced security with an integrated EdgeLock® Secure Enclave, a Physical Unclonable Function (PUF), On-The-Fly AES Decryption (OTFAD), a Trusted Resource Domain Controller (TRDC), a Battery Backed Security Module (BBSM), and an Inline Encryption Engine (IEE). The NXP i.MX RT1180 crossover MCUs feature an industrial temperature range of -40°C to +125°C.

The MIMXRT1180-EVK evaluation kit and the FRDM-IMXRT1186 development board, both also available from Mouser, provide extendable platforms to demonstrate the features of the NXP i.MX RT1180 MCUs. The Remote I/O Platform (RIOP) (PLCIOKIT) is designed to enable prototyping of high-precision data-acquisition and secure, multi-protocol connectivity solutions based on the NXP i.MX RT1180 series.

To learn more, visit https://www.mouser.com/new/nxp-semiconductors/nxp-i-mx-rt1180-crossover-mcus/.

For more Mouser news and our latest new product introductions, visit https://www.mouser.com/newsroom/.

 

As a global authorised distributor, Mouser offers the world's widest selection of the newest semiconductors and electronic components — in stock and ready to ship. Mouser's customers can expect 100% certified, genuine products that are fully traceable from each of its manufacturer partners. To help speed up the design process for customers, Mouser's website hosts an extensive library of technical resources, including a Technical Resource Centre, along with product data sheets, supplier-specific reference designs, application notes, technical design information, engineering tools and other helpful information.

About Mouser

2026 - Mouser Electronics is an authorized semiconductor and electronic component distributor focused on New Product Introductions from its leading manufacturer partners. Serving the global electronic design engineer and buyer community, the global distributor's website, mouser.com, is available in multiple languages and currencies and features more than 6.8 million products from over 1,200 manufacturer brands. Mouser offers 28 support locations worldwide to provide best-in-class customer service in local language, currency and time zone. The distributor ships to over 650,000 customers in 223 countries/territories from its 93,000m², state-of-the-art distribution facilities in the Dallas, Texas, metro area. For more information, visit https://www.mouser.com.

Trademarks

Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.

For further information, please contact:
Kevin Hess, Mouser
Senior Vice President of Marketing
+1 (817) 804-3833
For press enquiries, please contact:
Kelly DeGarmo, Mouser
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764