New at Mouser: onsemi AR0233AT Hayabusa CMOS Image Sensor for Automotive Applications

New Product Announcement

Connect With Us


Learn more about the AR0233AT image sensor
Learn more about the AR0233AT image sensor

May 5, 2026Mouser Electronics, Inc., the authorized global distributor with the newest electronic components and industrial automation products, is now shipping the new AR0233AT Hayabusa CMOS image sensor from onsemi. The AR0233AT delivers exceptional sensitivity for a wide variety of automotive and camera monitor system (CMS) applications, as well as machine vision applications.

The onsemi AR0233AT Hayabusa CMOS image sensor, available from Mouser, is built on a 3mm back-side-illuminated (BSI) pixel that features an active array size of 2048 x 1280 with 1080p output at 60 frames per second, providing greater than 140 dB of dynamic range in low-light conditions. The AR0233AT pixel technology includes LED flicker mitigation (LFM) while maintaining high dynamic range output, limiting the appearance of flicker from LED lighting and AC sources, which is particularly important for camera monitor systems (CMS) and machine vision algorithms. With requirements being added to the New Car Assessment Program (NCAP), advanced driver assistance systems (ADAS) require sensors to perform more complex algorithms at higher vehicle speeds in challenging lighting conditions for car safety. OEMs for automotive camera systems also seek to offer more features for customers by leveraging cameras for both viewing and sensing applications.

The AR0233AT sensor is available in multiple automotive-qualified package options, including iBGA and bare die. The components are ASIL-B safety-compliant, per ISO 26262, and support ASIL-B or higher safety ratings for camera systems. This sensor is also compatible with image signal processor (ISP) companion chips from onsemi and third-party ISPs.

To learn more, visit https://www.mouser.com/new/onsemi/onsemi-aro233at-image-sensors/. For more Mouser news and our latest new product introductions, visit https://www.mouser.com/newsroom/.

 

 

As a global authorised distributor, Mouser offers the world's widest selection of the newest semiconductors and electronic components — in stock and ready to ship. Mouser's customers can expect 100% certified, genuine products that are fully traceable from each of its manufacturer partners. To help speed up the design process for customers, Mouser's website hosts an extensive library of technical resources, including a Technical Resource Centre, along with product data sheets, supplier-specific reference designs, application notes, technical design information, engineering tools and other helpful information.

About Mouser

2026 - Mouser Electronics is an authorized semiconductor and electronic component distributor focused on New Product Introductions from its leading manufacturer partners. Serving the global electronic design engineer and buyer community, the global distributor's website, mouser.com, is available in multiple languages and currencies and features more than 6.8 million products from over 1,200 manufacturer brands. Mouser offers 28 support locations worldwide to provide best-in-class customer service in local language, currency and time zone. The distributor ships to over 650,000 customers in 223 countries/territories from its 93,000m², state-of-the-art distribution facilities in the Dallas, Texas, metro area. For more information, visit https://www.mouser.com.

About onsemi

2026 - onsemi is driving disruptive innovations to help build a better future. With a focus on automotive and industrial end markets, the company is accelerating change across megatrends such as vehicle electrification and safety, sustainable energy grids, industrial automation, and 5G and cloud infrastructure. onsemi offers a highly differentiated and innovative product portfolio, delivering intelligent power and sensing technologies that solve the world's most complex challenges and leads the way to creating a safer, cleaner, and smarter world. onsemi is recognized as a Fortune 500® company and included in the Nasdaq-100 Index® and S&P 500® index.

Trademarks

Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.

For further information, please contact:
Kevin Hess, Mouser
Senior Vice President of Marketing
+1 (817) 804-3833
For press enquiries, please contact:
Kelly DeGarmo, Mouser
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764