Phoenix Contact's PSRmodular XC Safety Modules, Now Available at Mouser, Monitor Safety in Extreme Ambient Conditions

New Product Announcement

Connect With Us


June 3, 2024Mouser Electronics, Inc., the authorized global distributor with the newest electronic components and industrial automation products, is now stocking the PSRmodular XC safety modules from Phoenix Contact. The PSRmodular XC Safety Modules minimize machine downtimes with comprehensive and easy-to-understand diagnostics. Suitable for use in harsh environments, the PSRmodular XC Safety Modules allow for faster resolution of safety incidents in process industry and maritime machinery applications.

The Phoenix Contact PSRmodular XC safety modules, now available at Mouser, meet stringent safety standards for reliable performance in a variety of industrial settings. The modules are TÜV, UL, and CSA certified and have several advanced approvals in preparation, including ATEX zone 2, heat treatment (EN 746, EN 298, and EN 50156), and UL Class 1, Div. 2. The PSRmodular XC safety modules operate effectively in a temperature range of -10ºC to +70ºC and feature corrosion protection with additional conformal coating on the printed circuit board.

The configurable PSRmodular XC small-scale controllers can monitor multiple safety functions within a single application. The modules can also be easily adapted to meet increased input/output port requirements, making them a versatile solution for expanding industrial needs. If there are not enough I/Os, the system can be extended on a modular basis with up to 18 safety-related extension modules. The additional modules are simply connected to the base module via the DIN rail connector. This provides extra I/Os for connecting more sensors and actuators. The PSRmodular XC safety modules can be easily configured using the PSRmodular software, requiring no programming skills. Users can set up the safety logic graphically with a drag-and-drop interface.

To learn more about the Phoenix Contact PSRmodular XC Safety Modules, visit https://www.mouser.com/new/phoenix-contact/phoenix-contact-psrmodular-xc-safety-modules/.

 

As a global authorised distributor, Mouser offers the world's widest selection of the newest semiconductors and electronic components — in stock and ready to ship. Mouser's customers can expect 100% certified, genuine products that are fully traceable from each of its manufacturer partners. To help speed up the design process for customers, Mouser's website hosts an extensive library of technical resources, including a Technical Resource Centre, along with product data sheets, supplier-specific reference designs, application notes, technical design information, engineering tools and other helpful information.

About Mouser

2026 - Mouser Electronics is an authorized semiconductor and electronic component distributor focused on New Product Introductions from its leading manufacturer partners. Serving the global electronic design engineer and buyer community, the global distributor's website, mouser.com, is available in multiple languages and currencies and features more than 6.8 million products from over 1,200 manufacturer brands. Mouser offers 28 support locations worldwide to provide best-in-class customer service in local language, currency and time zone. The distributor ships to over 650,000 customers in 223 countries/territories from its 93,000m², state-of-the-art distribution facilities in the Dallas, Texas, metro area. For more information, visit https://www.mouser.com.

About Phoenix Contact

2026 - Phoenix Contact is a global market leader and innovator in the electrical engineering and automation sectors. Founded in 1923, the family-owned company from Blomberg, Germany, now owns an international distribution network providing guaranteed proximity to its customers. Phoenix Contact offers innovative products and solutions around industrial connection technology, automation, interface systems and surge protection. The product range includes device connection technologies, sensors, controllers, modular terminal blocks, splash-proof machinery connectors, wireless Ethernet products for up-to-date control cabinets, and custom solutions for various applications.

Trademarks

Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.

For further information, please contact:
Kevin Hess, Mouser
Senior Vice President of Marketing
+1 (817) 804-3833
For press enquiries, please contact:
Kelly DeGarmo, Mouser
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764