Now at Mouser: TI’s BUF802 Buffering Op Amp Removes Complexity in Measurement DAQ Front Ends

New Product Announcement

Connect With Us


September 13, 2022Mouser Electronics, Inc., the industry’s leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components™, is now stocking the BUF802 high-speed buffering operational amplifier from Texas Instruments (TI). The BUF802 exponentially increases signal bandwidth in data acquisition systems, enabling design engineers to scale front-end designs across multiple data-acquisition applications for a variety of test and measurement applications, including oscilloscopes, active probes and high-frequency data-acquisition systems.

The TI BUF802, available from Mouser Electronics, is a high-input-impedance (Hi-Z), open-loop, unity gain buffer amplifier with a JFET-input stage that offers the industry’s widest bandwidth, capable of supporting frequency bandwidths up to 3.1 GHz. Replacing complex and costly ASIC-based design implementations, the BUF802 integrates features of discrete components in a single chip that increases bandwidth tenfold compared to FET-input amplifiers. This performance lets design engineers leverage higher signal throughput with minimal input settling time, leading to faster throughput and improved accuracy in higher-frequency signal measurement.

For development, Mouser also stocks the BUF802RGTEVM evaluation module, which features two separate signal configurations: a composite loop with a precision amplifier and the standalone BUF802 buffer. The BUF802RGTEVM features single or split supplies and footprints for SMA connectors into all analog inputs and outputs. Additionally, the layout is optimized to reduce parasitic coupling and provide the best signal fidelity across frequency.

To learn more about the BUF802 buffering amplifier, visit https://www.mouser.com/new/texas-instruments/ti-buf802-high-speed-op-amp/.

 

As a global authorised distributor, Mouser offers the world's widest selection of the newest semiconductors and electronic components — in stock and ready to ship. Mouser's customers can expect 100% certified, genuine products that are fully traceable from each of its manufacturer partners. To help speed up the design process for customers, Mouser's website hosts an extensive library of technical resources, including a Technical Resource Centre, along with product data sheets, supplier-specific reference designs, application notes, technical design information, engineering tools and other helpful information.

About Mouser

2026 - Mouser Electronics is an authorized semiconductor and electronic component distributor focused on New Product Introductions from its leading manufacturer partners. Serving the global electronic design engineer and buyer community, the global distributor's website, mouser.com, is available in multiple languages and currencies and features more than 6.8 million products from over 1,200 manufacturer brands. Mouser offers 28 support locations worldwide to provide best-in-class customer service in local language, currency and time zone. The distributor ships to over 650,000 customers in 223 countries/territories from its 93,000m², state-of-the-art distribution facilities in the Dallas, Texas, metro area. For more information, visit https://www.mouser.com.

Trademarks

Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.

For further information, please contact:
Kevin Hess, Mouser
Senior Vice President of Marketing
+1 (817) 804-3833
For press enquiries, please contact:
Kelly DeGarmo, Mouser
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764