Espressif Systems ESP32-C5 SoC, Now Available from Mouser, Delivers Affordable Wi-Fi 6 and Bluetooth Connectivity

New Product Press Brief

Connect With Us


Learn more about the ESP32-C5 SoC
Learn more about the ESP32-C5 SoC

March 11, 2026 - Mouser Electronics, Inc., the industry's leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components, is now stocking the ESP32-C5 Wi-Fi® and Bluetooth® Low Energy System-on-Chip (SoC) from Espressif Systems.

The ESP32-C5 SoC supports 2.4 GHz and 5.0 GHz dual-band Wi-Fi 6, Bluetooth LE 5, Zigbee® 3.0, and Thread 1.4. The SoC integrates a high-performance (HP) 32-bit RISC-V processor, a low-power (LP) 32-bit RISC-V processor, wireless baseband and MAC (supporting Wi-Fi, Bluetooth LE, and 802.15.4), an RF module, and multiple peripherals, with time-division coexistence among Wi-Fi, Bluetooth, and 802.15.4.

The Espressif ESP32-C5 SoC features 29 GPIOs and a comprehensive set of peripherals in a QFN package measuring 6 x 6 mm2. Security features include secure boot, flash and PSRAM encryption, cryptographic accelerators, Access Permission Management (APM) hardware block, and Physical Memory Protection (PMP).

The RSP32-C5 SoC is ideal for applications such as smart homes, industrial automation, medical wearables, smart agriculture, service robots, and IoT sensor hubs and data loggers.

The ESP32-C5-DevKitC-1 development kit, also available from Mouser, offers a demonstration and prototyping platform for the ESP32-C5 SoC. The development kit features USB Type-C® ports for power and programming, an onboard USB-to-UART bridge for easy debugging, and multiple GPIOs accessible via pin headers for peripheral integration. 

To learn more about the ESP32-C5 SoC, visit https://www.mouser.com/new/espressif/espressif-esp32-c5-socs/

For more Mouser news and our latest new product introductions, visit https://www.mouser.com/newsroom/.

 

As a global authorised distributor, Mouser offers the world's widest selection of the newest semiconductors and electronic components — in stock and ready to ship. Mouser's customers can expect 100% certified, genuine products that are fully traceable from each of its manufacturer partners. To help speed up the design process for customers, Mouser's website hosts an extensive library of technical resources, including a Technical Resource Centre, along with product data sheets, supplier-specific reference designs, application notes, technical design information, engineering tools and other helpful information.

About Mouser

2026 - Mouser Electronics is an authorized semiconductor and electronic component distributor focused on New Product Introductions from its leading manufacturer partners. Serving the global electronic design engineer and buyer community, the global distributor's website, mouser.com, is available in multiple languages and currencies and features more than 6.8 million products from over 1,200 manufacturer brands. Mouser offers 28 support locations worldwide to provide best-in-class customer service in local language, currency and time zone. The distributor ships to over 650,000 customers in 223 countries/territories from its 93,000m², state-of-the-art distribution facilities in the Dallas, Texas, metro area. For more information, visit https://www.mouser.com.

Trademarks

Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.

For further information, please contact:
Kevin Hess, Mouser
Senior Vice President of Marketing
+1 (817) 804-3833
For press enquiries, please contact:
Kelly DeGarmo, Mouser
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764