Pico Technology PicoScope 6428E-D Oscilloscope, Now at Mouser Electronics, Offers Superior Performance in Signal Analysis
June 19, 2024 - Mouser Electronics, Inc., the industry's leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components, is now stocking the PicoScope 6428E-D oscilloscope from Pico Technology.
Designed for users needing to capture, measure and analyze sub-nanosecond waveforms with critical precision, the PicoScope 6428E-D features 4 channels with four selectable input ranges (±50 mV, ±100 mV, ±200 mV, ±500 mV), a bandwidth up to 3 GHz, 100 ps time resolution and 4-gigasamples of buffer memory. The PicoSDK® (software development kit) provides drivers for Windows, macOS, and Linux as well as support code for external packages such as LabView and MathWorks. It also provides the capability to support the synchronizing of multiple units, through the 10 MHz input or aux trigger input. The PicoScope 6428E-D oscilloscope also features streaming mode, allowing for continuous data capture directly to a PC with the capture size limited only by the available storage. This makes it an ideal tool for system integration applications and original equipment manufacturers.
Applications for the PicoScope 6428E-D include high-energy physics, particle accelerators, light detection and ranging (LIDAR), velocity-interferometer systems for any reflector (VISAR), spectroscopy, and medical imaging.
To learn more, visit https://www.mouser.com/new/pico-technology/pico-picoscope-6428e-d-oscilloscope/.
As a global authorised distributor, Mouser offers the world's widest selection of the newest semiconductors and electronic components — in stock and ready to ship. Mouser's customers can expect 100% certified, genuine products that are fully traceable from each of its manufacturer partners. To help speed up the design process for customers, Mouser's website hosts an extensive library of technical resources, including a Technical Resource Centre, along with product data sheets, supplier-specific reference designs, application notes, technical design information, engineering tools and other helpful information.
2026 - Mouser Electronics is an authorized semiconductor and electronic component distributor focused on New Product Introductions from its leading manufacturer partners. Serving the global electronic design engineer and buyer community, the global distributor's website, mouser.com, is available in multiple languages and currencies and features more than 6.8 million products from over 1,200 manufacturer brands. Mouser offers 28 support locations worldwide to provide best-in-class customer service in local language, currency and time zone. The distributor ships to over 650,000 customers in 223 countries/territories from its 93,000m², state-of-the-art distribution facilities in the Dallas, Texas, metro area. For more information, visit https://www.mouser.com.
Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.