Mouser Electronics Now Shipping Analog Devices LTC2688 16-Channel DAC for Optical Networking, Automation

New Product Announcement

Connect With Us


October 5, 2021Mouser Electronics, Inc., the industry’s leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components™, is now stocking the LTC2688 SoftSpan™ digital-to-analog converter (DAC) from Analog Devices, Inc. The LTC2688 provides engineers with advanced capability, efficiency and programmability for a variety of optical networking, automation, and telecom applications.

The Analog Devices LTC2688, available from Mouser Electronics, is a 16-channel, 16-bit DAC with integrated precision reference to improve the accuracy of the outputs. The DAC features independently programmable channels, with five output ranges from 0 V up to ±15 V. Offering monotonic stability, the LTC2688 includes built-in rail-to-rail output buffers that can source or sink up to ±20 mA.

The LTC2688 also offers external reference for additional range options and an analog multiplexer to simplify measurement of pin voltages, load currents, and junction temperature. The serial peripheral interface (SPI) and MICROWIRE™-compatible, 3-wire serial interface operates on logic levels as low as 1.71 V and clock rates up to 50 MHz.

The LTC2688 is supported by the DC2873A-B evaluation board, also available from Mouser. The DC2873A-B is a fully featured evaluation board that, when paired with the required DC2026C demo board, enables designers to use Analog Devices’ Analysis, Control, Evaluation (ACE) software to configure and control the onboard LTC2688 DAC.

To learn more about the LTC2688 DAC, visit https://www.mouser.com/new/analog-devices/adi-ltc2688-dac/.

 

As a global authorised distributor, Mouser offers the world's widest selection of the newest semiconductors and electronic components — in stock and ready to ship. Mouser's customers can expect 100% certified, genuine products that are fully traceable from each of its manufacturer partners. To help speed up the design process for customers, Mouser's website hosts an extensive library of technical resources, including a Technical Resource Centre, along with product data sheets, supplier-specific reference designs, application notes, technical design information, engineering tools and other helpful information.

About Mouser

2026 - Mouser Electronics is an authorized semiconductor and electronic component distributor focused on New Product Introductions from its leading manufacturer partners. Serving the global electronic design engineer and buyer community, the global distributor's website, mouser.com, is available in multiple languages and currencies and features more than 6.8 million products from over 1,200 manufacturer brands. Mouser offers 28 support locations worldwide to provide best-in-class customer service in local language, currency and time zone. The distributor ships to over 650,000 customers in 223 countries/territories from its 93,000m², state-of-the-art distribution facilities in the Dallas, Texas, metro area. For more information, visit https://www.mouser.com.

About Analog Devices Inc.

2026 - Analog Devices, Inc. operates at the center of the modern digital economy, converting real-world phenomena into actionable insight with its comprehensive suite of analog and mixed signal, power management, radio frequency (RF), and digital and sensor technologies. ADI serves 125,000 customers worldwide with more than 75,000 products in the industrial, communications, automotive, and consumer markets. ADI is headquartered in Wilmington, MA. Visit http://www.analog.com.

Trademarks

Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.

For further information, contact:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
+1 (817) 804-3833
For press enquiries, contact:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764