Mouser Now Shipping Qorvo QPD0011 GaN-on-SiC HEMT for 4G & 5G Communications

New Product Announcement

Connect With Us


August 9, 2021Mouser Electronics, Inc., the industry’s leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components, is now stocking the QPD0011 high-electron mobility transistor (HEMT) from Qorvo®. The gallium nitride-on-silicon carbide (GaN-on-SiC) transistor delivers power and performance for cellular base station and RF applications in 5G massive MIMO, LTE, and WCDMA systems.

The Qorvo QPD0011, available from Mouser Electronics, is an asymmetric, dual-path amplifier in a small, 7.0 mm × 6.5 mm DFN package. Utilizing variable power inputs from 30 W to 60 W and drain voltages of +48 V, the QPD0011 operates between 3.3 GHz and 3.6 GHz and features up to 13.3 dB of gain, for ultra-efficient signal, peak, and power performance (up to 90 W) in Doherty design environments.

For development, Mouser also stocks the QPD0011EVB1 Evaluation Board. The QPD0011EVB1 platform includes an example application circuit, allowing rapid prototyping when incorporated into existing designs. Applications for the QPD0011 include macrocell and microcell base stations, active antennas, and asymmetric Doherty designs.

To learn more about the QPD0011 GaN-on-SiC HEMT, visit https://www.mouser.com/new/qorvo/qorvo-qpd0011-48v-gan-sic-hemt/.

 

As a global authorised distributor, Mouser offers the world's widest selection of the newest semiconductors and electronic components — in stock and ready to ship. Mouser's customers can expect 100% certified, genuine products that are fully traceable from each of its manufacturer partners. To help speed up the design process for customers, Mouser's website hosts an extensive library of technical resources, including a Technical Resource Centre, along with product data sheets, supplier-specific reference designs, application notes, technical design information, engineering tools and other helpful information.

About Mouser

2026 - Mouser Electronics is an authorized semiconductor and electronic component distributor focused on New Product Introductions from its leading manufacturer partners. Serving the global electronic design engineer and buyer community, the global distributor's website, mouser.com, is available in multiple languages and currencies and features more than 6.8 million products from over 1,200 manufacturer brands. Mouser offers 28 support locations worldwide to provide best-in-class customer service in local language, currency and time zone. The distributor ships to over 650,000 customers in 223 countries/territories from its 93,000m², state-of-the-art distribution facilities in the Dallas, Texas, metro area. For more information, visit https://www.mouser.com.

Trademarks

Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.

For further information, please contact:
Kevin Hess, Mouser
Senior Vice President of Marketing
+1 (817) 804-3833
For press enquiries, please contact:
Kelly DeGarmo, Mouser
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764