Renesas CK-RA6M5 Cloud Kit, Now at Mouser, Features Multiple Onboard Sensors for Home and Building Automation
July 25, 2023 – Mouser Electronics, Inc., the authorized global distributor with the newest semiconductors and electronic components, is now stocking the CK-RA6M5 cloud kit from Renesas Electronics. Based on the RA6M5 32-bit microcontroller group, the CK-RA6M5 cloud kit features a broad range of onboard sensors, including temperature, humidity, barometric pressure, and environmental air quality. The cloud kit is ideal for home and building automation, smart cities, healthcare and industrial monitoring applications.
The Renesas CK-RA6M5 cloud kit, now available at Mouser, features LTE CAT-M1 and Ethernet network connectivity interfaces, while a broad range of add-on devices support additional cloud connectivity options. The CK-RA6M5 cloud kit includes two MEMS microphones for voice command applications and SpO2 and indoor/outdoor AQI sensors. The compact cloud kit also features an onboard debugger (J-LINK or E2OB) and an Arduino Uno interface. The cloud kit also includes the popular Digilent Pmod (Type 2A and Type 6A) connectors to add other sensors or connectivity options such as motion sensors, Bluetooth® Low Energy or Wi-Fi®. It also has USB Full Speed and USB Serial ports.
The CK-RA6M5 cloud kit is supported by a comprehensive software suite, including a complete software stack using Renesas software packages, Flexible Software Package, and the new IoT Quick Connect Studio platform.
Amazon Web Service (AWS) and Microsoft Azure cloud applications are also supported, and the integrated generic applications are cloud agnostic. These applications use a feature-rich custom dashboard to visualize the sensor data on the cloud kit.
To learn more about the CK-RA6M5 cloud kit, visit https://www.mouser.com/new/renesas/renesas-rtk7cka6m-kit/.
As a global authorised distributor, Mouser offers the world's widest selection of the newest semiconductors and electronic components — in stock and ready to ship. Mouser's customers can expect 100% certified, genuine products that are fully traceable from each of its manufacturer partners. To help speed up the design process for customers, Mouser's website hosts an extensive library of technical resources, including a Technical Resource Centre, along with product data sheets, supplier-specific reference designs, application notes, technical design information, engineering tools and other helpful information.
2026 - Mouser Electronics is an authorized semiconductor and electronic component distributor focused on New Product Introductions from its leading manufacturer partners. Serving the global electronic design engineer and buyer community, the global distributor's website, mouser.com, is available in multiple languages and currencies and features more than 6.8 million products from over 1,200 manufacturer brands. Mouser offers 28 support locations worldwide to provide best-in-class customer service in local language, currency and time zone. The distributor ships to over 650,000 customers in 223 countries/territories from its 93,000m², state-of-the-art distribution facilities in the Dallas, Texas, metro area. For more information, visit https://www.mouser.com.
Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.