Mouser Electronics Now Shipping Renesas' Ultra-Small DA14535 SmartBond TINY SoC, Ideal for Medical Disposables

New Product Announcement

Connect With Us


Learn more about the DA14535 SmartBond TINY SoC
Learn more about the DA14535 SmartBond TINY SoC

July 14, 2025Mouser Electronics, Inc., the authorized global distributor with the newest semiconductors and electronic components, is now stocking the DA14535 SmartBond TINY system-on-chip (SoC) from Renesas Electronics. The low-power, cost-effective DA14535 is one of the industry's smallest and most power-efficient Bluetooth® 5.3 SoCs, enabling new classes of Internet of Things (IoT) devices, including the growing market for connected medical products.

The DA14535 SmartBond TINY SoC, available from Mouser Electronics, achieves a low system cost through a high level of integration. The SoC is based on a 32-bit Arm® Cortex®-M0+ microcontroller with a complete set of analog and digital peripherals and incorporates a 2.4 GHz transceiver in a minuscule form factor of just 2.2 × 3.0 mm. By adding just six external passives, a crystal oscillator, a power source, plus a 2.4GHz antenna, designers can build a complete Bluetooth Low Energy system for applications such as asset tracking and proximity tags, wireless sensor nodes, wearables, medical, human interface devices (HID), industrial appliances, and more.

Mouser also stocks the DA14535MOD SmartBond TINY BLE 5.3 module, based on the DA14535 SoC. The low-power module is worldwide certified and features an integrated 1 Mbit NOR Flash, a 32 MHz XTAL and a printed antenna, enabling a faster time to market at reduced development costs.

The DA14535 SmartBond TINY development kits, also available at Mouser, enable rapid demonstration and evaluation of the DA14535 SoC and are available in USB and Pro versions. The DA14535 USB kit is a small, portable USB board with Bluetooth Low Energy technology, one mikroBUS connector, 2 Mbits of SPI flash, and an onboard DA14535 SoC. The DA14535 Pro kit includes a motherboard, a daughterboard with the DA14535 SoC, and a mini-USB cable. The kit's extensive features include two mikroBUS header interfaces, Arduino Uno compatibility, and onboard 2-Mbit SPI data flash. The DA14535 Pro kit allows users to perform RF measurements using an embedded printed antenna and SMA connector capability.

To learn more, visit https://www.mouser.com/new/renesas/renesas-dialog-da14535-soc/.

For more Mouser news and our latest new product introductions, visit https://www.mouser.com/newsroom/.

 

As a global authorised distributor, Mouser offers the world's widest selection of the newest semiconductors and electronic components — in stock and ready to ship. Mouser's customers can expect 100% certified, genuine products that are fully traceable from each of its manufacturer partners. To help speed up the design process for customers, Mouser's website hosts an extensive library of technical resources, including a Technical Resource Centre, along with product data sheets, supplier-specific reference designs, application notes, technical design information, engineering tools and other helpful information.

About Mouser

2026 - Mouser Electronics is an authorized semiconductor and electronic component distributor focused on New Product Introductions from its leading manufacturer partners. Serving the global electronic design engineer and buyer community, the global distributor's website, mouser.com, is available in multiple languages and currencies and features more than 6.8 million products from over 1,200 manufacturer brands. Mouser offers 28 support locations worldwide to provide best-in-class customer service in local language, currency and time zone. The distributor ships to over 650,000 customers in 223 countries/territories from its 93,000m², state-of-the-art distribution facilities in the Dallas, Texas, metro area. For more information, visit https://www.mouser.com.

About Renesas Electronics

2026 - Renesas Electronics is a semiconductor company with an outstanding portfolio of global market-leading products. Renesas has the technology and capabilities to deliver almost everything required in an age focusing on human needs, including security technologies, miniaturization and power-saving technologies, networking, and interface technologies. Renesas aims to stay one step ahead and to be the true intelligent chip solution provider — the world leader in its field.

Trademarks

Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.

For further information, contact:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
+1 (817) 804-3833
For press enquiries, contact:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764