Renesas FS1015 & FS3000 Air Flow Sensor Modules Now Shipping from Mouser

New Product Announcement

Connect With Us


October 12, 2021Mouser Electronics, Inc., the industry’s leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components™, is now stocking the FS1015 and FS3000 air flow sensor modules Renesas Electronics. The vertical-mount FS1015 and the surface-mount FS3000 provide precision air flow monitoring for detecting system failures, measuring air handling, controlling fan speed, and more in HVAC systems, analytic gas-monitoring systems, data centers, and air quality systems.

The FS1015 and FS3000 sensors, now shipping from Mouser, use a series of MEMS thermocouples to provide high-sensitivity air monitoring. Both sensors measure direct local air at up to 15 meters per second, allowing system control to adjust quickly, providing closed-loop control while achieving maximum efficiency and cost savings. The solid thermal isolation of the MEMS sensing element combined with a silicon-carbide film offers excellent abrasive wear resistance and long-term reliability.

The FS1015 comes in a 28.2 mm × 14.2 mm × 7.3 mm package with leads for vertical mounting and screw-secured side tabs. The FS3000 module is available in an 8.0 mm × 9.1 mm × 4.4 mm surface-mount package ideal for low-profile applications.

For more information about the FS1015 module, visit https://www.mouser.com/new/renesas/renesas-fs1015-air-velocity-sensor-module/.

To learn more about the FS3000 module, go to https://www.mouser.com/new/renesas/renesas-fs3000-air-velocity-sensor-module/.

 

As a global authorised distributor, Mouser offers the world's widest selection of the newest semiconductors and electronic components — in stock and ready to ship. Mouser's customers can expect 100% certified, genuine products that are fully traceable from each of its manufacturer partners. To help speed up the design process for customers, Mouser's website hosts an extensive library of technical resources, including a Technical Resource Centre, along with product data sheets, supplier-specific reference designs, application notes, technical design information, engineering tools and other helpful information.

About Mouser

2026 - Mouser Electronics is an authorized semiconductor and electronic component distributor focused on New Product Introductions from its leading manufacturer partners. Serving the global electronic design engineer and buyer community, the global distributor's website, mouser.com, is available in multiple languages and currencies and features more than 6.8 million products from over 1,200 manufacturer brands. Mouser offers 28 support locations worldwide to provide best-in-class customer service in local language, currency and time zone. The distributor ships to over 650,000 customers in 223 countries/territories from its 93,000m², state-of-the-art distribution facilities in the Dallas, Texas, metro area. For more information, visit https://www.mouser.com.

Trademarks

Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.

For further information, please contact:
Kevin Hess, Mouser
Senior Vice President of Marketing
+1 (817) 804-3833
For press enquiries, please contact:
Kelly DeGarmo, Mouser
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764