Mouser Now Stocking Sensirion SEN5x Environmental Sensor Nodes for Reliable Air Quality Data

New Product Announcement

Connect With Us


May 3, 2022 Mouser Electronics, Inc., the industry's leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components™, is now stocking the SEN5x environmental sensor nodes from Sensirion. Optimized with multiple sensing parameters, the SEN5x nodes enable designers to save valuable R&D, BOM and assembly costs by providing an all-in-one sensor solution that replaces multiple environmental sensors.

The Sensirion SEN5x environmental sensor nodes, available from Mouser Electronics, help improve end customers’ health and comfort by accurately measuring and reporting the levels of relevant indoor pollutants in particulate matter, volatile organic compounds (VOCs), oxidizing gases (NOx and O3), humidity and temperature in a variety of air quality applications. The advanced sensors offer easy integration, fully calibrated outputs with a digital interface, and superior measurement of vital air quality parameters in a single device versus multiple sensor components. The sensor nodes provide one driver for up to eight data signals and perform all operations and communications through an I²C interface.

The SEN5x nodes feature integrated proprietary measurement algorithms, including VOC/NOx index calculation, humidity compensation, and temperature compensation, which enable straightforward integration into HVAC and air quality applications. Along with the temperature compensation engine, the devices also incorporate a Sensirion Temperature Acceleration Routine (STAR) engine, which accelerates the devices’ response to ambient temperature changes by a factor of two to three.

The sensor nodes offer a lifetime of over 10 years and are available in a compact 52.8 mm × 43.6 mm × 22.3 mm form factor. For evaluation and development, Mouser also stocks the SEK-SEN5x evaluation kit.

To learn more about the Sensirion SEN5x environmental sensor nodes, visit https://www.mouser.com/new/sensirion/sensirion-sen5x/.

 

As a global authorised distributor, Mouser offers the world's widest selection of the newest semiconductors and electronic components — in stock and ready to ship. Mouser's customers can expect 100% certified, genuine products that are fully traceable from each of its manufacturer partners. To help speed up the design process for customers, Mouser's website hosts an extensive library of technical resources, including a Technical Resource Centre, along with product data sheets, supplier-specific reference designs, application notes, technical design information, engineering tools and other helpful information.

About Mouser

2026 - Mouser Electronics is an authorized semiconductor and electronic component distributor focused on New Product Introductions from its leading manufacturer partners. Serving the global electronic design engineer and buyer community, the global distributor's website, mouser.com, is available in multiple languages and currencies and features more than 6.8 million products from over 1,200 manufacturer brands. Mouser offers 28 support locations worldwide to provide best-in-class customer service in local language, currency and time zone. The distributor ships to over 650,000 customers in 223 countries/territories from its 93,000m², state-of-the-art distribution facilities in the Dallas, Texas, metro area. For more information, visit https://www.mouser.com.

About Sensirion

2026 - Sensirion is a leading sensor manufacturer, providing relative humidity sensors and flow sensor solutions with unique performance. The company's product range includes liquid flow sensors, mass flow meters, mass flow controllers and differential pressure sensors. Using Sensirion's microsensor solutions, OEM customers benefit from the proven CMOSens® technology and excellent technical support. Among a large variety of applications, flow and humidity sensors are successfully used in the automotive and medical industries.

Trademarks

Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.

For further information, please contact:
Kevin Hess, Mouser
Senior Vice President of Marketing
+1 (817) 804-3833
For press enquiries, please contact:
Kelly DeGarmo, Mouser
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764