TDK InvenSense's IIM-42653 SmartIndustrial MotionTracking Device, Now at Mouser, Delivers Reliable Precision in Industrial Applications

New Product Announcement

Connect With Us


August 27, 2024Mouser Electronics, Inc., the authorized global distributor with the newest electronic components and industrial automation products, is now stocking the IIM-42653 SmartIndustrial™ MotionTracking device from TDK InvenSense. The 6-axis MEMS device provides precise, reliable motion-tracking capabilities in industrial applications. The IIM-42653 is optimized for performance and power efficiency in challenging environments, and applications include navigation, orientation measurements, platform stabilization, and robotics.

The TDK InvenSense IIM-42653 SmartIndustrial MotionTracking device, now available at Mouser, integrates a 3-axis gyroscope and a 3-axis accelerometer into a compact 2.5 mm x 3 mm x 0.91 mm package. The IIM-42653, which features an operating temperature range of -40°C to +105°C, is 20,000g shock tolerant. The device supports an extended full-scale range of up to 32g and 4000dps, suitable for demanding industrial conditions. The IIM-42653 features a 2KBytes FIFO that reduces energy consumption by allowing the system processor to read sensor data and then switch to low-power mode. The sensor supports a highly accurate external clock input that is beneficial for robotics, tilt sensing, and other applications that require precise navigation and orientation measurements. For communication, the IIM-42653's host interface can support i3CSM, I2C, and SPI modes, with respective maximum speeds of 12.5MHz, 1MHz, and 24MHz. The I3CSM interface also supports speeds up to 25 Mbps in DDR mode. The IIM-42653 device has an operating voltage range of 1.71V to 3.6V.

The IIM-42653 is supported by the TDK InvenSense DK-42653 development kit. The DK-42653 features an onboard embedded debugger and necessary software, including InvenSense Motion Link, a GUI-based development tool, and embedded motion drivers.

To learn more, visit https://www.mouser.com/new/tdk/tdk-iim-42653-smartindustrial-motiontracking-device/.

 

As a global authorised distributor, Mouser offers the world's widest selection of the newest semiconductors and electronic components — in stock and ready to ship. Mouser's customers can expect 100% certified, genuine products that are fully traceable from each of its manufacturer partners. To help speed up the design process for customers, Mouser's website hosts an extensive library of technical resources, including a Technical Resource Centre, along with product data sheets, supplier-specific reference designs, application notes, technical design information, engineering tools and other helpful information.

About Mouser

2026 - Mouser Electronics is an authorized semiconductor and electronic component distributor focused on New Product Introductions from its leading manufacturer partners. Serving the global electronic design engineer and buyer community, the global distributor's website, mouser.com, is available in multiple languages and currencies and features more than 6.8 million products from over 1,200 manufacturer brands. Mouser offers 28 support locations worldwide to provide best-in-class customer service in local language, currency and time zone. The distributor ships to over 650,000 customers in 223 countries/territories from its 93,000m², state-of-the-art distribution facilities in the Dallas, Texas, metro area. For more information, visit https://www.mouser.com.

About InvenSense

2026 - InvenSense, Inc., a TDK Group company, is a world leading provider of MEMS sensor platforms. InvenSense's vision of Sensing Everything® targets the consumer electronics and industrial areas with integrated motion and sound solutions. InvenSense's solutions combine MEMS (micro-electrical-mechanical systems) sensors, such as accelerometers, gyroscopes, compasses, and microphones with proprietary algorithms and firmware that intelligently process, synthesise, and calibrate the output of sensors, maximising performance and accuracy. InvenSense's motion tracking, audio and location platforms, and services can be found in mobile, wearables, smart home, industrial, automotive, and IoT products. In May of 2017, InvenSense became part of the MEMS Sensors Business Group within the newly formed Sensor Systems Business Company of TDK Corporation. InvenSense is headquartered in San Jose, California, and has offices worldwide.

Trademarks

Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.

For further information, contact:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
+1 (817) 804-3833
For press enquiries, contact:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764