Mouser Now Shipping Texas Instruments DLP2021-Q1 DLP Digital Micromirror Device for Automotive and EV Applications

New Product Announcement

Connect With Us


August 7, 2024Mouser Electronics, Inc., the authorized global distributor with the newest electronic components and industrial automation products, is now stocking the new DLP2021-Q1 automotive 0.2" DLP® digital micromirror device (DMD) from Texas Instruments. The DLP2021-Q1 is designed for automotive exterior light control and display applications that include ground projection in full color with animated and dynamic content for automotive and EV applications.

The TI DLP2021-Q1 DLP DMD, available from Mouser, is designed for automotive exterior light control and display applications with full color and animated dynamic content. These tiny devices can be placed in many locations throughout the car, including inside the side mirror, door panel, taillight, front grill and more to facilitate vehicle-to-pedestrian (V2P) communication such as back-up, door-open, and other vehicle communication warning systems and vehicle personalization options. Due to the device's small form factor and low-power operation, projectors with the DLP2021-Q1 chipset can support many projection applications.

The DLP2021-Q1 chipset can be coupled with LEDs or lasers to create highly saturated colors with over 125 percent of the National Television System Committee (NTSC) color gamut. It can be used with either RGB or white illumination sources. A DLP2021-Q1 field-programmable gate array (FPGA) configuration is provided and is used to drive the DLP2021-Q1 automotive DMD. This controller architecture is designed for small form factor projectors and does not require a video bus or graphics processing unit (GPU) for content creation. Video and image content is stored on local flash and can be played at power-up or on command.

The DLP2021-Q1 is supported by the DLP2021LEWQ1EVM evaluation module, also available from Mouser. The DLP2021LEWQ1EVM brings together a set of components, including the DLP2021-Q1 DMD, the FPGA-based DMD controller, and the TPS65100 PMIC, to provide an efficient system for evaluation of dynamic ground projection technology.

To learn more, visit https://www.mouser.com/new/texas-instruments/ti-dlp2021-q1-automotive-dlp-dmd/.

 

 

As a global authorised distributor, Mouser offers the world's widest selection of the newest semiconductors and electronic components — in stock and ready to ship. Mouser's customers can expect 100% certified, genuine products that are fully traceable from each of its manufacturer partners. To help speed up the design process for customers, Mouser's website hosts an extensive library of technical resources, including a Technical Resource Centre, along with product data sheets, supplier-specific reference designs, application notes, technical design information, engineering tools and other helpful information.

About Mouser

2026 - Mouser Electronics is an authorized semiconductor and electronic component distributor focused on New Product Introductions from its leading manufacturer partners. Serving the global electronic design engineer and buyer community, the global distributor's website, mouser.com, is available in multiple languages and currencies and features more than 6.8 million products from over 1,200 manufacturer brands. Mouser offers 28 support locations worldwide to provide best-in-class customer service in local language, currency and time zone. The distributor ships to over 650,000 customers in 223 countries/territories from its 93,000m², state-of-the-art distribution facilities in the Dallas, Texas, metro area. For more information, visit https://www.mouser.com.

About Texas Instruments

2026 - Texas Instruments Incorporated is a global semiconductor company that designs, manufactures, and sells analog and embedded processing chips for markets such as industrial, automotive, personal electronics, enterprise systems, and communications equipment. At its core, Texas Instruments has a passion to create a better world by making electronics more affordable through semiconductors. This passion is alive today as each generation of innovation builds upon the last to make the company's technology more reliable, more affordable, and lower power, making it possible for semiconductors to go into electronics everywhere.

Trademarks

Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.

For further information, please contact:
Kevin Hess, Mouser
Senior Vice President of Marketing
+1 (817) 804-3833
For press enquiries, please contact:
Kelly DeGarmo, Mouser
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764