Vishay RAIK060 Rotational Absolute Inductive Kit Encoders, Now at Mouser, Enable Automation, Motor Drives and Robotics

New Product Announcement

Connect With Us


Month 06, 2025Mouser Electronics, Inc., the authorized global distributor with the newest electronic components and industrial automation products, is now stocking RAIK060 rotational absolute inductive kit encoders from Vishay. Designed specifically for the accurate positioning of motor drives, industrial robotics and industrial motion control, the RAIK060 is a patented, off-axis rotational absolute inductive kit encoder that provides high repeatability, precision and high resolution in a single or multi-turns variant.

Vishay RAIK060 encoders, available from Mouser Electronics, deliver rotation speeds up to 10,000 rpm and a latency time of less than or equal to 5 µs to allow for faster motor drive calculation processes. The repeatability of these position sensors is specified at greater than or equal to 17 bits, with overall accuracy at 13 bits and an encoder resolution of 18 bits. To increase reliability, the RAIK060 offers built-in self-monitoring and memorization of its last position before powering off. Available outputs of the RAIK060 include an SPI, SSI and BiSS-C interface with single and multi-turn variants. Other notable features include embedded self-calibration, a useful 360° electrical mechanical angle and easy assembly flexibility through status LED colors.

Built for operating in even the harshest environments, RAIK060 encoders are not sensitive to moisture, pollution, temperature, vibrations or shock. The encoders are also insensitive to external magnetic fields (no Hall effect cells), electrical fields and temperature, making them ideal for designs that require close proximity to electrical motors. RAIK060 encoders feature a compact, space-saving and lightweight chassis-mount form factor, measuring only 60 mm in diameter, 5 mm in thickness and less than 15 g in weight.

To learn more, visit https://www.mouser.com/new/vishay/vishay-raik060-encoders/.

 

As a global authorised distributor, Mouser offers the world's widest selection of the newest semiconductors and electronic components — in stock and ready to ship. Mouser's customers can expect 100% certified, genuine products that are fully traceable from each of its manufacturer partners. To help speed up the design process for customers, Mouser's website hosts an extensive library of technical resources, including a Technical Resource Centre, along with product data sheets, supplier-specific reference designs, application notes, technical design information, engineering tools and other helpful information.

About Mouser

2026 - Mouser Electronics is an authorized semiconductor and electronic component distributor focused on New Product Introductions from its leading manufacturer partners. Serving the global electronic design engineer and buyer community, the global distributor's website, mouser.com, is available in multiple languages and currencies and features more than 6.8 million products from over 1,200 manufacturer brands. Mouser offers 28 support locations worldwide to provide best-in-class customer service in local language, currency and time zone. The distributor ships to over 650,000 customers in 223 countries/territories from its 93,000m², state-of-the-art distribution facilities in the Dallas, Texas, metro area. For more information, visit https://www.mouser.com.

About Vishay

2026 - Vishay manufactures one of the world’s largest portfolios of discrete semiconductors and passive electronic components that are essential to innovative designs in the automotive, industrial, computing, consumer, telecommunications, military, aerospace, and medical markets. Serving customers worldwide, Vishay is The DNA of tech.™ Vishay Intertechnology, Inc. is a Fortune 1,000 Company listed on the NYSE (VSH).

Trademarks

Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.

For further information, please contact:
Kevin Hess, Mouser
Senior Vice President of Marketing
+1 (817) 804-3833
For press enquiries, please contact:
Kelly DeGarmo, Mouser
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764