Intel Quark SoC X1000 Processors Now in Stock at Mouser
March 11, 2014 – Mouser Electronics, Inc. is now shipping the new Intel® Quark X1000 System‑on‑a‑Chip (SoC), the latest Intel 32-bit processor built for the next generation of connected devices. The Quark X1000 is the first in a new line of Intel processors designed for new applications ranging from Internet‑of‑Things (IoT) to wearables, transportation, energy, and industrial control.
The new Intel Quark X1000 SoC Processors available from Mouser Electronics run as fast as 400MHz and are designed specifically for high performance low power applications. The Quark is backwards‑compatible with previous Intel processors and software compatible with existing x86‑based CPUs such as the Intel Atom™ and Intel Core™ line of processors. The Quark is 100% compatible with the Pentium® instruction set and even runs PC compatible software.
Performance is enhanced with 16Kbytes of shared instruction and L1 data cache, improving code execution speeds by minimizing the number of times the CPU needs to access external memory. 512Kbytes of on‑chip SRAM is also available.
The Intel Quark SoC boasts a variety of on-chip connectivity which includes a PCI Express interface, two 10/100‑Ethernet ports, USB 2.0 Enhanced Host Controller Interface (EHCI), USB 2.0 Open Host Controller Interface (OHCI), I2C, SPI, and a high speed UART with DMA.
The Intel Quark supports a variety of external memory interfaces including microSD™, SDIO, and eMMC. An on-chip DDR3 memory controller allows easy access and control of external DRAM memory.
To learn more about Intel's latest Quark X1000 processor, visit:
http://www.mouser.com/new/Intel/intel-quark-x1000/
With its broad product line and unsurpassed customer service, Mouser caters to design engineers and buyers by delivering What's Next in advanced technologies. Mouser offers customers 20 global support locations and the latest, most technologically advanced components for their newest design projects. Mouser Electronics' website is updated daily and searches more than 10 million products to locate over 4 million orderable part numbers available for easy online purchase. Mouser.com also houses an industry-first interactive catalog, data sheets, supplier-specific reference designs, application notes, technical design information, and engineering tools.
About Mouser Electronics
Mouser Electronics, a subsidiary of TTI, Inc., is part of Warren Buffett's Berkshire Hathaway family of companies. Mouser is an award-winning authorized semiconductor and electronic component distributor, focused on the rapid introduction of new products and technologies to electronic design engineers and buyers. Mouser.com features more than 4 million products online from more than 500 manufacturers. Mouser publishes multiple catalogs per year providing designers with up-to-date data on the components now available for the next generation of electronic devices. Mouser ships globally to over 400,000 customers in 170 countries from its 492,000 sq. ft. state-of-the-art facility south of Dallas, Texas. For more information, visit www.mouser.com.
About Intel
Intel is the world’s largest manufacturer of semiconductors and has established a heritage of innovation that continues to expand the reach and promise of computing while advancing the ways people work and live worldwide. Intel’s entire processor portfolio provides design engineers with direct access to the industry’s most advanced processors. Intel’s industry-leading technologies are created using the most advanced foundry process technologies in the industry, producing unprecedented levels of performance and efficiency.
Trademarks
Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.
Further information, contact:
Kevin Hess, Mouser Electronics
Vice President Technical Marketing
(817) 804-3833
Kevin.Hess@mouser.com
For press inquiries, contact:
Kevin Parmenter, Mouser Electronics
Director of Technical Resources
(817) 804-7926
Kevin.Parmenter@mouser.com