Finland - Flag Finland

Incoterms:DDP
All prices include duty and customs fees on select shipping methods.

Please confirm your currency selection:

Euros
Free shipping on most orders over 75 € (EUR).

US Dollars
Free shipping on most orders over $90 (USD).

Bench Talk for Design Engineers

Bench Talk

rss

Bench Talk for Design Engineers | The Official Blog of Mouser Electronics


Math: the Language of Engineers, Scientists, and Artists Alike Lynnette Reese
Neil Armstrong’s favorite quote was "Science is about what is, engineering is about what can be.” STEM, and now STEAM (Science, Technology, Engineering, Art, and Mathematics) promote these areas for growth. Some might consider the “Art” in STEAM to be out of place, but I disagree. Engineers need cross-pollination, and have you seen some of the incredible art using open source technology?

Self-Driving Cars Offer Interesting Transportation Possibilities Caroline Storm Westenhover
According to some published studies, the area has the 10th worst traffic in the U.S. and the longest average commute in the US. I have given extensive thought to the social ramifications of self-driving cars. I have thought about this many times before, but now it is personal. The technology used in self-driving cars is fascinating, but I want to talk about the implications.

Circuit Protection – Why Bother?? Kelly Casey
Let’s face it - circuit protection can be a tough sell. Here’s why: 1) Circuit protection isn’t sexy. It doesn’t add any “wow factor to the product." 2) In fact, it doesn’t add any functionality to the product at all. 3) Any effect circuit protection has on the function of a device is likely negative. Adding capacitance, resistance or potential non-linearity to an I/O port is rarely useful in promoting high data rates. 4) It adds cost and can increase complexity. What circuit protection does do is provide some measure of reliability. It gives the end product the ability to sustain and likely survive potentially damaging electrical surges or contact with unexpectedly high voltages without exposing the user to electrical shock or becoming a fire hazard.

RF Power Transistors and the Mystery of Video Bandwidth Barry Manz
If you use RF power transistors, you may have come across a new term of late on the datasheets: video bandwidth (VBW). Now, anyone who uses spectrum analyzers knows about this key metric, but I’ve been poring over power transistor datasheets for years, and this one seemed to appear out of nowhere.

Road-Tripping on Thermodynamics Caroline Storm Westenhover
My family is mildly crazy and the stunt for this past Spring was driving from Los Angeles to Indianapolis in 72 hours. One of my brothers was graduating in Los Angeles and another was getting married near Indianapolis. About 90 minutes out of LA, our car overheated. Naturally my mom and I decided to open the hood and see what we could do. As I poured water over the radiator, I noticed that in some spots the water was boiling on contact and other places it was rolling off and dripping onto the ground. I thought about my thermal class. In particular I was thinking of thermal contact resistance. I recalled a particularly illustrative picture from Chapter 10 of my thermal book and the heat conduction of road dust versus metal (Hint: it is not helping with the heat transfer).

Give Your Next OSHW Project Some Android Love Mike Parks
Android, iOS tablets, and smartphones revolutionized the idea of the User Interface (UI). These devices are intuitive, powerful, and omnipresent in our daily lives. So instead of reinventing the wheel for a slick UI to control your next OSHW project, why not simply build the interface as an app? Typically the answer is that creating apps isn't quite as simple as using apps.

OTA Software Updates for Your Car?! John Donovan
Now here’s a scary thought: You’re driving down the freeway in heavy traffic when the LCD screen in your dashboard that was previously displaying a song title suddenly informs you that the firmware for your car’s 100+ electronic control units (ECUs) has been updated wirelessly and you need to reboot your car for them to take effect. What happens if you’re distracted and don’t press the No button soon enough? If your car were my PC it would reboot automatically. Not so good at 70 mph.

All Authors

Show More Show More
View Blogs by Date

Archives